Associating a Standard Graphic to an Equipment Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and standard graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.

To associate a Standard graphic to an Equipment object in SCT:

Procedure

  1. Select the Equipment object in the Equipment tree.
  2. If graphics are not already associated to device objects, then go to the Configuration tab of the Equipment object and click Edit.
  3. Select the Standard graphic from the All Items tree. Drag the Standard graphic to the Graphic attribute field.
    Note: You can have several graphics associated to an Equipment object.
  4. Click Save.