Associating Standard Graphics - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Note: In Metasys® UI 2.1 and later, you can associate Standard graphics to spaces or equipment in the Graphics Manager of the Metasys UI or Metasys UI Offline. You can also associate Metasys UI graphics to spaces, equipment, or Equipment Definitions. For more information, refer to Metasys® UI Help (LIT-12011953) or Metasys® UI Offline Help (LIT-12012116) .