Associating a Graphics+ Graphic to an Equipment Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Graphics+ graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.

To associate a Graphics+ graphic to an Equipment object in SCT:

Procedure

  1. Select the Equipment object in the Equipment tree.
  2. In the Configuration tab of the Equipment object, click Edit.
  3. Select the Graphics+ graphic from the All Items tree. Drag the Graphics+ graphic to the Graphic attribute field.
    Note: You can have several graphics associated to an Equipment object.
  4. Click Save.