Enabling Advanced Auditing - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

At Metasys UI Release 2.0 and later, the Equipment Activity widget captures audits of commands performed by Schedule objects, Multiple Command objects, and Interlock objects that are tied to equipment configured to the Metasys UI. To utilize this feature, the Engine object must be at Metasys Release 8.0 or later and the Enable Application Generated Audits attribute must be set to True.

Procedure

  1. In SCT , open the Engine object's Configuration tab.
  2. Select Advanced.
  3. Click Edit.
  4. Under the Audit Trail section, change the Enable Application Generated Audits value to True.
  5. Click Save and perform a download to update the online configuration of the device.