Using the Spaces Tree Editor - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

To begin configuring your Metasys site into spaces, go to Facility > MUI Config > Edit Spaces Tree.

You can create spaces for your Spaces Tree using one of three methods:
  • Manually add each space using the buttons described in Table 1.
  • Drag folders from a User View into the Spaces Tree.
  • Create multiple spaces at once by using a spreadsheet.
Figure 1. Spaces Tree Editor Buttons

In the Spaces Tree Editor, click Edit. The button bar appears. Table 1 describes the Spaces Tree Editor's button bar functionality.

Table 1. Spaces Tree Editor Buttons

Button

Description

Save a Spaces Tree

Cancel editing or adding a Spaces Tree

Add new space (space object) to Spaces Tree

Remove selected Spaces Tree object

Move selected Spaces Tree object up in the tree

Move selected Spaces Tree object down in the tree

Sort Spaces Tree in ascending order

Sort Spaces Tree in descending order