Download Archive on Site Director for Spaces Tree - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

Before you can browse to the Metasys UI on a client device, you must first download your archive to the ADS/ADX Site Director.
Note: The Download function is required for the initial setup of Spaces and Equipment for a site. After you create a base set of Spaces and Equipment on a site, you can use the Download Only Metasys UI Spaces and Equipment feature to make the updates.

Procedure

  1. Click Tools > Manage Archive.
  2. Select Download to Device and click Next.
  3. Follow the prompts in the Manage Archive wizard.
  4. Browse to the Metasys UI on a client device. The web address is https://[Host Name or IP address]/UI, where [Host Name or IP address] is the server name or server IP address.