Equipment Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

An Equipment object is created through the Facility > MUI Config > Discover Equipment option and through equipment discovery when creating Equipment Definitions. Equipment objects are listed in the Equipment tree in SCT. This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.

Note: In the Notes column, attributes marked with the letter C are configurable and attributes marked with the letter W are writeable.
Table 1. Equipment Object – Focus/Configuration Tab

Attribute Name

Data Type

Notes

Initial Value

Values/Options/Ranges

Name

Text

C

 

Maximum length of 400 characters

Description

Text

C

 

Maximum length of 64 characters

Object Type One type from a set C Equipment Undefined

Authorization Category

One type from a set

C

HVAC

HVAC, Fire, Security, Services, Administrative, General Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System Custom 1–150

Served By

List of

C

Listof[0]

 

Definition Link

Reference

C

Blank or Object Name and Reference of Equipment Definition

Blank or Object Name and Reference of Equipment Definition

Graphic

Object Reference

C W

 

Blank or Object Name and Reference

Graphic Alias Reference Strings (fully qualified references)    

Maximum 256 characters