Serving Match Tolerance - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The default value for Serving Match Tolerance is 0.95, which you can set in the frameworkproperties.properties file located under C:\inetpub\wwwroot\MetasysIII\ToolUI\com\jci\framework. The value needs to be between 0.0 and 1.0, where a smaller number may return a greater number of incorrect matches.

Clicking Rediscover Spaces provides a slider bar for adjusting Serving Match Tolerance. The slider bar has a range of 0% to 100% with a default value that correlates with the range of 0.0 to 1.0 and the default value in the frameworkproperties.properties file.

If you are not satisfied with the results generated by following the Find and Replace to Assist Auto-Discovery Serving Relationships workflow, follow these steps to adjust Serving Match Tolerance.

  1. Right-click on the Serving column heading or a row and select Rediscover Spaces.
  2. Use Ctrl+click or Shift+click to select the rows that are missing the serving relationship.
  3. Drag the value on the slider bar from the default. A smaller number increases the likelihood of finding a new serving relationship, but may return a greater number of incorrect matches.
    Note: This changes default value for the active session. After logging out and closing the SCT user interface, the default will revert to the value assigned in the frameworkproperties.properties file.
  4. When you release the slider bar, the software automatically rediscovers spaces and update the Serving column. You may continue to change the value using the slider bar until satisfactory relationships have been discovered.
    Note: If you do not have rows selected when you release the slider the software automatically rediscovers spaces for all rows.