|
Step |
Description |
|---|---|
| 1 |
Click an Equipment Definition in the All Items Tree. |
| 2 |
Open an Equipment Discovery (). |
| 3 | Click the Add icon to add Field Controllers to the Equipment Discovery Window. |
| 4 | Click OK to populate the Equipment Discovery window. |
| 5 |
For single edits: Click one equipment object row, and then right-click the column heading to select Find and Replace (in selection). For multiple edits: Ctrl+click or click and drag across one or more rows to create a selection. Then right-click the column heading to select Find and Replace (in selection). For full column edits: Right-click the column heading and select Find and Replace. |
| 6 |
Enter the criteria for the Find field and the Replace field. To replace all matching text, select Matching Text. To replace all non-matching text, select Non-Matching Text. Figure 1. Replace All
|
| 7 | Click Replace All. |
|
Character |
Search Description and Application |
|---|---|
| An asterisk (*) |
Use before and after the search criteria text to search that portion of the text. For example, *ZN-T*. Use in the search criteria text lets you search for zero or more of any character. For example, Z*-T returns results including ZN-T and ZONE-T. |
| A question mark (?) |
Use in the search criteria text to search for zero or one instance of any character. For example, Hum?-C returns results including Hum1-C and Hum-C. |
| A percent symbol (%) |
Use in the search criteria text to search for numerals 0 through 9. For example, Hum%-C returns results including Hum1-C and Hum7-C. You can enter multiple % to search for text that contains multiple numerals. For example, Hum%%-C returns results including Hum26-C. This also matches the percent symbol itself, such as in: % Humidity. |
| A pound sign (#) |
Use in the search criteria text to search for a string of one or more numerals. For example, #BoxHtg-C returns results including 1BoxHtg-C and 34BoxHtg-C. This search also matches the pound sign itself, such as in: BLDG #1. |
| Normal Text |
Use in the search criteria to return results that match the characters exactly without matching case. For example, zn-t returns results for ZN-T and zn-t. |