Delete Items - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Edit > Delete Items

Deletes one or more items selected in the All Items tree from the site.

Note: The Edit menu or Right-click > Delete functions are not used to delete items from a User View while the User View Editor is open. Using either function permanently deletes selected items from the archive.

For details on deleting items, see Deleting Objects or Items.