Modify Dialog Box - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Modify dialog box allows you to modify attributes of a single item in the Metasys system. You can access the Modify dialog box for the selected item by selecting the Modify menu option from the Action Menu or the right-click menu. The attributes shown in the modify box are different for different object types.

Figure 1. Modify Dialog Box

Table 1. Modify Dialog Box Components

Screen Area/Item

Description

Instructions Area

Provides tips to help you send a modification.

Attributes Table

Displays the list of attributes available to modify for the selected item. Unauthorized modifications are disabled. Attribute value fields appear after the attribute name.

The check box next to an attribute is automatically selected when you make a modification in its value field. Modifications are sent for only the selected (checked) attributes.

Send

Sends the selected modifications to the object/item.

Cancel

Closes the Modify dialog box without sending the changes.