Modify Attributes - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The following table lists the attribute groupings and examples of the attributes available for modification.

Note: You can easily enter each controller's Fully Qualified Reference (FQR) by entering an asterisk (*) in the Graphic Alias field.
Table 1. Modify Attributes

Attribute Grouping

Example Attributes

General

  • Change of Value (COV) Increment
  • Display Precision
  • Authorization Category
  • Units

BACnet Intrinsic Alarming

  • BACnet Deadband
  • High Limit
  • Low Limit

Alarm Values

  • Differential
  • High Alarm Limit
  • Low Alarm Limit

Alarm Setup

  • Alarm Ack Required
  • Alarm Message Text
  • Alarm Priority
  • Event Enable

Graphic Setup

  • Graphic
  • Graphic Alias