Event Totalization - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Event Totalization extension tracks the number of binary events or pulses over time, meaning it counts the number of transitions that occur at an input reference. Unlike other types of totalization, event totalization increases the value each time the event occurs, instead of calculating the value once each minute.

These three essential parameters determine the mode of operation for the Event Totalization extension:

  • the monitored Input Reference

  • the types of recorded Transitions or events

  • the recorded Value Per Pulse (event)

You can use this extension to determine the number of changes in an input value, which may be helpful for maintaining and monitoring equipment. For example, use Event Totalization to determine how many times a motor started, how often a sensor was in alarm, or how many cars entered a parking lot.

For detailed information on the Event Totalization extension, see Event Totalization Attributes.