Runtime Totalization Attributes - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The Runtime Totalization extension contains attributes common to Metasys system objects. For details, see Common Object Attributes.

The following table lists the attributes specific to the Runtime Totalization extension. Click the attribute name in the table for a description of the attribute.

Note: In the Notes column, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Runtime Totalization Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Display Precision

C,W

10ths

Uses Display Precision (Set 0).

Executing

 

Active

See Executing.

Active

Totalize Limit

Inactive

Active: The extension is calculating and has not reached the Totalize Limit.

Totalize Limit: The extension has reached the limit and has stopped calculating because Rollover is set to False.

Inactive: The extension is unreliable or disabled and is not calculating.

Input Reference

C

   

Present Value

C,D,R,W

   

Reference

C,W

State 1

States Test attribute identifies the enumeration set for this attribute.

Reliability

 

Reliable

Uses Reliability (Set 503).

Reset

(This attribute does not appear in a view, but may be scheduled, trended, and so on.)

W

False

False

True

Reset Date

     

Reset Time

     

Rollover

C,W

False

False

True

Rollover Count

R,W

0

0–4,294,967,295

States Text

(This attribute does not appear in a view, but may be scheduled, trended, and so on.)

C,W

States

See States Text.

Timebase

C,W

Hours

Seconds, minutes, hours, days

Totalize Limit

C,N,W

Hours

 

Units

C,W

No Units

 

Value Before Reset