The following table indicates the file containing resources located within the host computer.
|
Element Name |
Initial Value |
Values/Options/Range |
Description |
|---|---|---|---|
|
Exportable |
False |
Available in a future release |
Indicates whether you can export the file. If True, you can export the file. If False, you cannot export the file. This element of the File Name attribute is to be available in a future release. |
|
Object References |
Indicates the object references embedded in the file. |
||
|
References |
False |
Indicates whether the file has references. If True, the file has references. If False, the file has no references. |
|
|
Relative Path |
Size = 100 Category = Default |
Indicates the file name of the file relative to the directory containing the MOI file for the device. |