Resource File Extensions contain attributes common to Metasys system objects. For details, see Common Object Attributes.
The following table lists the attributes specific to the Resource File extension. Click the attribute name in the table for a description of the attribute. Attributes marked with the letter C are configurable, and attributes marked with the letter W are writable.
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
Description |
---|---|---|---|---|
File Name |
C |
Category = File |
See the File Name section. |
|
Information |
C,W |
Size = 80 Category = Default |
Indicates the text you assigned to provide further information about the resource file. This attribute can be written to from an integration server after reading the resource file. |