Load Command Interactions - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Table 1 illustrates command interactions that pertain to Load objects.

Table 1. Load Command Interactions

Load Command(s) Currently in Effect

Load Command Not Allowed

Explanation

Shed

Shed

Load cannot be shed because it is already shed.

Shed + Locked

Comfort Override

or

Release Load

Lock must be removed with Unlock command.

Comfort Override

Shed

Comfort Override must be released with Release Comfort Override command.

Released + Locked

Shed

Lock must be removed with Unlock command.

Released + Locked

and

Comfort Override

Shed

Comfort Override must be released with Release Comfort Override command.

Lock must be removed with Unlock command.