About this task
Notes:
- You cannot delete an extension in online mode with Basic Access.
- For a trend extension that is configured to automatically transfer data to an Metasys Server or ODS (Repository Enabled = True), be sure to route unforwarded data to the Metasys Server or ODS before deleting the trend extension. If you do not, unforwarded trend data is lost.
Procedure
-
To delete extensions (using the Navigation Tree):
- Select the item from the navigation tree and select Show Extensions from the Action menu.
- Select the check box of the extension you want to delete.
- Click Delete.
-
To delete extensions (when the item is in the Panel Layout):
- View the extension.
- Select the tab for the extension.
- Select the extension.
- Click Delete.