Creating Extensions - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

Notes:

  • You cannot create an extension in online mode with Basic Access.
  • You can add only one load extension to an object.
To create extensions:

Procedure

  1. Select the item from the Navigation Tree and select Show Extensions from the Action menu.
    Note: Alternatively, you can create extensions when prompted upon completion of a wizard, or when the item is in the Panel Layout by selecting the tab for the extension and clicking new.
  2. Select New for the type of extension that you want to create. The corresponding Extension Wizard appears.
  3. Select the attribute that you want to associate with the item.
  4. Complete the information on the wizard screens. The screens vary depending on the type of extension you are creating.
  5. Select Finish on the summary page to create the extension.