Averaging Commands - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The following table lists the commands supported by the Averaging Extensions. Click the command name for a description of the command.

Table 1. Averaging Extension Commands

Command Name

Parameters

Description

Enable

None

Disable

None

Clear

None