Alarm Extensions - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Alarm extensions monitor an attribute of an object and send alarms using the Alarm and Event Management feature. There are two types of alarm extensions, Analog Alarm and Multistate Alarm. Use the Analog Alarm extension to monitor attributes with real values. Use the Multistate Alarm extension to monitor attributes with True or False, or Multistate data types.

For general information on Metasys system objects, see the Object Help section.