Extension Wizard - Metasys - LIT-12011964 - MS-SCTRMOT-0 - MS-SCTSWO-0 - MS-SCTSWO-6 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020
Note: You cannot add or delete extensions in Simulation mode.

Menu Selection: Actions > Show Extensions (menu option is available only when an item that supports extensions is selected)

Adds features, such as trending, alarming, averaging, loading and totalization, to an item. Extension types include:

  • Resource File—Adds a resource file to a field device or integration, if supported.
  • Trend—Adds trending capabilities to an item.
  • Totalization—Adds totalization capabilities to an item.
    Note: Select either the Event Totalization or Runtime Totalization radio button if they appear on the right side of the Select Attribute screen of this wizard. If these selections do not appear, the attribute you selected uses Analog Totalization.
  • Alarm—Adds attributes for generating alarm and event messages to an item. For more information, refer to the Alarm and Event section of the Metasys SMP Help (LIT-1201793).
  • Averaging—Adds averaging capabilities to an item.
  • Load—Adds the load capability of the Energy Management feature. You can add only one load extension to an object.

See the Extensions section.