Import Integration - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Action > Import Integration

This command is only available when an Integration under an engine is selected in the All Items tree. After adding an Integration, you can select the integration in the navigation tree and use this menu selection to add existing devices and points under the integration.