Import Definition - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Action > Import Definition

Imports the pre-built summary definition that is stored on the computer and is only available when the Summary Definitions folder is selected in the All Items tree. After importing a definition, the imported Summary Definitions appear in the Summary Definitions folder in the All Items tree.

Note: You also can import Summary Definitions that were previously exported.