Action Menu - Feature Specific - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The following table describes the different menu items that appear in the Action menu based on the active panel or feature displayed in the selected display panel. Click each active panel or feature for a description. For more information on the modes of operation, see Metasys Modes.

Note: The Refresh, Refresh Current Tab, and Refresh All Tabs menu items appear in the Action menu for all other features or active panels.
Table 1. Action Menu - Feature Specific

Active Panel/Feature

Contents In Mode

Online (Standard Access)

Online (Basic Access)

Offline (SCT)

Event Viewer

  • Refresh
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Ack
  • Discard
  • Refresh
 

Audit Viewer

  • Refresh
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Clear Audit Log
   

ActionQ

   
  • Refresh

Tailored Summary Viewer

The menu options available are item-specific (that is, they depend on the type of item selected in the Summary Definitions and Key Data tables).

  • Command
  • Modify
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Show Extensions
  • Remove From Site (available for a network engine only).
  • Import Integration (available for a Tailored Summary with trunk/integration data. For example, trunk diagnostics).
  • Command
  • Modify
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
 

Global Search

  • Refresh

  • Refresh
 

Change Results Viewer

No Action menu options for this feature.