Action Menu - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

In addition to the four modes of operation that determine the items appearing in menus, the Action menu is context specific. Different item specific options appear in the Action menu based on what is currently selected in the navigation tree. Also, different feature specific options appear in the Action menu based on the active panel or feature displayed in the selected display panel.

Note: The options available in the Action Menu are also accessible through the right-click functionality.