User settings - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

To access the Users settings, from the main menu, click Settings > User settings.

Use the User settings window to add or delete the users that can access MRE Web Interface. You can grant administrator or guest permissions to a user.

To use the MRE from the Metasys User Interface, set the Login mode to MSEA.