Running report definitions - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

After you save the report definition, it appears in the main window’s tree.

To enable the group, right-click on the node, and click Enabled.

The runtime status of the report is displayed with the following icons:
  1. Report creation status is unknown: indicates a problem in the MRE service.
    Figure 1. Report creation status is unknown
  2. Report creation process is disabled: indicates that no reports are being generated. For a one-shot report it may indicate that the report has already been generated.
    Figure 2. Report creation process is disabled
  3. Report creation process is enabled and waiting to create the report at the time date and time set at the report definition process.
    Figure 3. Report creation process is enabled and waiting to create the report
  4. Report creation process is running and the report is being created. When you hover the mouse cursor over the report node, a tooltip with the progress information appears.
Figure 4. Report is being created