Report definitions editor: general tab - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
In the General tab, the following settings are available:
  1. Report definition information
  2. Type
  3. Connection
    1. SQL Connection parameters for Trend, Event, Audit and SQL Historian Trend reports
    2. M-Data folder for Access Historian Trend reports
    3. EDE Connection for Trend reports
  4. Data Format only for Trend and M-Collector Trend reports
  5. Options only for Trend and M-Collector Trend reports
  6. Output