Options - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
The Options pane contains the following setting for Trend, Access Historian Trend and SQL Historian Trend reports:
  • N+1 Samples: select to create reports for energy consumption computation. When you select this option, a further sample is added to the report. For example, when you do not select the N+1 samples option and the Sample Time is 15 minutes, a daily report adds the last sample at 23:45. However, when you select the N+1 samples option, the last sample in the report is taken at 0:00 of the next day, thus allowing energy computation as the difference between the sample taken at 0:00 of the next day and the sample taken at 0:00 of the current day.
  • Collection Period: defines a sub-interval within the collection period. Use one of the following modes:
    • Classic Mode: enter the period when you want the data sampled. For example, if a daily report starting at 6:00 AM is configured and the Collection Period is set to 8 hours, the report includes only samples from 6:00 AM to 2:00 PM. The data from 2:00 PM to 6:00 AM of the following day is discarded.
    • Gold Mode: You can select for each day of the week the intervals that you want data sampled. To configure the intervals, click the Edit schedule button.