Field positions - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English

The Field positions group allows user to select the cell where data needs to copied to.

Use the Field positions pane to select the cells that you want to enter data.

For Trends and M-Collector Trend reports, you can also add a header to the report. Select the header format from the Compile header using list. The Compile header using list contains the following options:
  • None
  • Point full name: inserts the item fully qualified into to the row entered in the field positions grid
  • Point user name: inserts the item user name into the row entered in the field positions grid. Available for only Trends reports.
  • Full name + user name: inserts the item fully qualified name into the row entered in the field positions grid. Inserts the user name into the row immediately below. Available for only Trends reports.

To insert the point description in the report, select the Insert description checkbox. The Insert description option is not available for M-Collector Trend reports.

You can select to insert the data in either a vertical or horizontal direction.