Report conversion - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

Report conversion converts old report definition files to work with later versions of Metasys.

Select the report you want to update and use with a Trend DataBase, coming from a Metasys installation.

Use report conversion when you update an older version of Metasys ADX/ADS and the MRE was already installed with reports configured.

When you convert a report, a backup of the original is saved in the BKP_ConvertedReports folder found in the MRE Application Data.

Note: The conversion is done using the XML Dictionary file, available in the configured folder from the MRE System Settings. It is possible to have more than one file in the same folder.