Registering Metasys Report Engine - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English
To check if your copy of the MRE is registered, from the MRE start up window, click Help > About.The following figure shows an example of the About window with a registered copy of the MRE.
Figure 1. Registered copy of the MRE
Figure 2. MRE start-up window

When you use an unregistered version of the MRE, some capabilities are disabled. For example, reports are filled with invalid values (999)

To register your copy of the MRE, see Licensing MRE Application.

After you install the MRE, you can find a MRE icon in the system tray.

To minimize the MRE to the system tray, click File > <Minimize. To restore the MRE main window, double-click the MRE icon.