Folder definition - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

Use the folder definition to define a multi-level structure and organize the reports definition according to a specific request.

Figure 1. MRE folder structure

The structure automatically replicates under the root folder into specific report types, such as Trends, Events, and Audit, in order to have the same result when the report type changes.

You can delete empty folders from the menu.