Disabled performance counters - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

Condition

After you create a MRE group with Excel .xls file generation, the report does not generate.

The MRE Report Log for groups displays the following message:
…
Successfully connected to Metasys
5/12/2008 16.02.39 - Waiting for Excel availability...
5/12/2008 16.02.39 - Unexpected error: Process performance counter is disabled, so the requested operation cannot be performed.
5/12/2008 16.02.39 - Report creation terminated

Cause:

The System Monitor Performance Counters are disabled.

Solution:

To enable the System Monitor Performance Counters, refer to the following Microsoft documentation https://www.betaarchive.com/wiki/index.php?title=Microsoft_KB_Archive/248993.