IIS Configuration Check for Web Version - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English

About this task

After you install the MRE standalone and MRE Web Version, check that the Internet Information Services Manager settings are configured correctly.

Procedure

  1. From the Control Panel window, click System and Security > Administrative Tools > Internet Information Services (IIS) Manager.
  2. In the Features View pane, click ISAPI and CGI Restrictions.
  3. Make sure that the Restriction values for ASP.NET v4.0 are set to Allowed.
    Figure 1. ISAPI and CGI restrictions
  4. In the Connections navigation tree, click Application Pools.
  5. In the Application Pools pane, right-click MRE_AppPool and click Advanced Settings. Make sure that the parameters in the General section match the following figure.
    Figure 2. Application Pool settings
  6. From the Connections tree, under Sites > Default Web Site right-click MREService site, and right click selecting Manage Application -> Advanced Settings. Make sure that all the parameters in the General section match the following figure.
    Figure 3. MREService settings