The new web user interface is divided into two sections. The reports tree is located on the left side of the screen and facilitates the navigation through the reports. The report parameters definition is located on the left side of the screen and facilitates the navigation through the Spaces, Network, and Views tabs.
All the user interface components are equal to the standard MRE user
interface. The report tree is the same and also all the reports parameters are the
same.
Figure 1. Web client user interface
Clicking on a report it is possible to open the report definition with all the parameters. To see all the parameter information, see Report definitions editor.
The available operation for each report are:
- Add a report into a specific folder
- Clone an existing report
- Save report definition (after editing)
- Enable (execute) a report
- Delete an existing report
- Download the output file (XLS, CSV or PDF) produced by a report
- Create a folder
- Delete a folder
All the operations are available according to the user restriction set using MRE User Settings.