Report definition tabs - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active

The report definition tabs are located on the right side of the home screen and facilitates the navigation through the reports.

Report definition tabs are composed by three different tabs:
  1. General tab.
  2. Point / Attributes selection.
  3. Additional parameters. Visible when the output file is set to Excel.
Figure 1. General tab
Figure 2. Points/attributes selection tab
Figure 3. Additional parameters tab