Open Web MRE from Metasys UI - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English

You can add Web MRE to the Metasys UI using the Metasys UI Graphics Manager. From Graphics Manager you can add an item, such as a button, and edit the button to link to the Web MRE login page with a hyperlink. For example, https://xxx.xxx.xxx.xxx/MREService. For detailed information about creating and editing Metasys UI graphics, refer to the Graphics Manager section of the Metasys UI Help (LIT-12011953).

Figure 1. MRE link on UI page