Launching Web MRE from the SMP Interface - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English

Procedure

  1. Launch Metasys Site Management Portal (SMP).
  2. Click Tools > Configure Preferences > Applications.
  3. Click Add.
  4. Select System application if all the users have the possibility to run the external application. In other cases the procedure is to log in with all the users authorized and add the external application as User.
    • If you want all unauthorized users to run the external application, select System application.
    • If you want all authorized users to run the external application, add the external application as User.
  5. Enter the Application name: MRE Web client.
  6. Enter the Web MRE path iexplore.exe “https://xxx.xxx.xxx.xxx/MREService” where xxx.xxx.xxx.xxx is the IP address or the computer name of the computer where MRE service is installed.
  7. Click OK.