To run MRE requires the following hardware and software resources:
- Windows 10 Professional 64
- Windows Server Standard Edition 2012/2016/2019
- NET framework 4.7+ or later
- 100 MB minimum of free disk space
- Metasys ADS/ADX version 6.5 or later. Metasys OAS.
Note: Windows Server Datacenter is not supported.
Note:
You can use MRE with older
versions of Metasys such as 6.5, however for optimal performance use MRE with
supported versions of Metasys. The supported versions of Metasys are the latest and
the previous release.