Installing PDFCreator - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Brand
Metasys
Product name
Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
Language
English

About this task

To create reports in PDF format, complete the following steps:

Procedure

  1. Download the PDFCreator from https://www.pdfforge.org/pdfcreator/download.
  2. Run the PDFCreator Setup.exe file.
  3. Select I accept the license agreement and click Next.
  4. Select Standard Installation and click Next.
  5. In the Printer name window, click Next.
  6. In the Select Destination Location screen, choose the installation folder location and click Next.
  7. In the PDFCreator toolbar screen, click Next.
  8. In the Select components window, make sure that you uncheck the PDFCreator toolbar for Internet Explorer and Firefox options. Click Next.
  9. In the Select Start Menu folder field, enter the folder name and click Next.
  10. In the Select Additional tasks window, click Next.
  11. Click Install.
  12. Click Finish.