Filename rule - Metasys - LIT-12014183 - Software Application - Metasys Advanced Reporting System - 3.0

Metasys Report Engine User Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System
Document type
User Guide
Document number
LIT-12014183
Version
3.0
Revision date
2023-03-06
Product status
Active
The following table describes the DATE_TIME_FORMAT rules:
Table 1. Format tags
Format tag Description
d

Displays the current day of the month, measured as a number between 1 and 31, inclusive. If the day is a single digit only (1-9), then it is displayed as a single digit.

When you use the 'd' format specifier alone, without other custom format strings, it is interpreted as the standard short date pattern format specifier. If the 'd' format specifier is passed with other custom format specifiers or the % character, it is interpreted as a custom format specifier.

dd Displays the current day of the month, measured as a number between 1 and 31, inclusive. If the day is a single digit only (1-9), it is formatted with a preceding 0 (01-09).
ddd Displays the abbreviated name of the day.
dddd Displays the full name of the day for the specified
h Displays the hour in the range 1-12. The hour represents whole hours passed since either midnight (displayed as 12) or noon (also displayed as 12). If this format is used alone, then the same hour before or after noon is indistinguishable. If the hour is a single digit (1-9), it is displayed as a single digit
hh Displays the hour in the range 1-12. The hour represents whole hours passed since either midnight (displayed as 12) or noon (also displayed as 12). If this format is used alone, then the same hour before or after noon is indistinguishable. If the hour is a single digit (1-9), it is formatted with a preceding 0 (01-09).
H Displays the hour in the range 0-23. The hour represents whole hours passed since midnight (displayed as 0). If the hour is a single digit (0-9), it is displayed as a single digit.
HH Displays the hour in the range 0-23. The hour represents whole hours passed since midnight (displayed as 0). If the hour is a single digit (0-9), it is formatted with a preceding 0 (01-09).
m Displays the minute in the range 0-59. The minute represents whole minutes passed since the last hour. If the minute is a single digit (0-9), it is displayed as a single digit.
mm Displays the minute in the range 0-59. The minute represents whole minutes passed since the last hour. If the minute is a single digit (0-9), it is formatted with a preceding 0 (01-09).
M Displays the month, measured as a number between 1 and 12, inclusive. If the month is a single digit (1-9), it is displayed as a single digit.
MM Displays the month, measured as a number between 1 and 12, inclusive. If the month is a single digit (1-9), it is formatted with a preceding 0 (01-09).
MMM Displays the abbreviated name of the month
MMMM Displays the full name of the month
s Displays the seconds in the range 0-59. The second represents whole seconds passed since the last minute. If the second is a single digit (0-9), it is displayed as a single digit only.
ss Displays the seconds in the range 0-59. The second represents whole seconds passed since the last minute. If the second is a single digit (0-9), it is formatted with a preceding 0 (01-09).
t Displays the first character of the A.M./P.M. designator
tt Displays the A.M./P.M. designator
y Displays the year as a maximum two-digit number. The first two digits of the year are omitted. If the year is a single digit (1-9), it is displayed as a single digit.
yy Displays the year as a maximum two-digit number. The first two digits of the year are omitted. If the year is a single digit (1-9), it is formatted with a preceding 0 (01-09).
yyyy Displays the year, including the century. If the year is less than four digits in length, then preceding zeros are appended as necessary to make the displayed year four digits long.
: Time separator.
/ Date separator.
" Quoted string. Displays the literal value of any string between two quotation marks preceded by the escape character (/).
' Quoted string. Displays the literal value of any string between two " ' " characters.
Any other character Other characters are written directly to the result string as literals.