Updating the scan - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.3

Metasys Performance Verification Tool (PVT) User Guide

Brand
Metasys
Product name
Performance Verification Tool
Document type
User Guide
Document number
LIT-12012406
Version
4.3
Revision date
2023-07-27
Language
English

About this task

You can update the list of supervisory devices in the scan and then restart the scan. For example, you can include the points of additional supervisory devices in the scan data.

To update a scan, complete the following steps:

Procedure

  1. Click Open Scan in the toolbar or main menu, or click on the card of a recent scan in the main PVT window.
  2. Click Update Scan in the upper right.
  3. Enter your user name and password.
  4. In the supervisory device list, select the check box next to a device to add the device to the scan, or clear the check box next to a device to exclude the device from the scan.
  5. Click Scan Selected.