The main PVT user interface contains the following options: New Scan, Open Scan and Compare Scans. Use the menu icon with three lines in the top left corner of the interface to access these options and also the following options: Delete Scan, Preferences, Settings, Help, and About.
Figure 1. PVT user interface in interactive mode
Option | Description | |
---|---|---|
New Scan | Open the New Project interface to create a new project. | |
Open Scan | Open an existing project from the local database or from a
PVT file. Note: You can open PVT files from PVT version 3.0 and
above.
|
|
Delete Scan | Delete an existing project from your local system. | |
Compare Scans | Compare two projects from different points in time to identify any changes in site data. | |
Preferences | Tab | Description |
Field Point | Modify the point names search criteria for better point results. | |
Instance Number | Modify the instance number search criteria for better point results. | |
Equipment Type | Modify the equipment type names search criteria for better point results on equipment identification. | |
Rule Preferences | Modify rule preferences for scheduling, setpoints, filters, alarm events, user management, thermal waste, fan motor, and different modules of variation form set points. | |
Settings | Modify language settings and work hours information. Enable or disable sync status. | |
Help | View PVT documentation in browser. | |
About |
View version and license information for your PVT installation. Check the latest rule version synced from the cloud. |