About this task
When you open a scan, you can export a riser diagram of the scanned devices into a Microsoft Visio file.
Note: This function is available only for inventory and
performance scans. You must have Microsoft Visio 2013 or above installed for this
process to work.
Procedure
- Open a scan. Click Open Scan in the toolbar or main menu, or click on the card of a recent scan in the main PVT window.
- Click Export Riser in the upper right.
- Microsoft Visio opens and the riser diagram is automatically created.