You can enable or disable syncing to the cloud in Automatic scan mode or Interactive mode. The Sync status is set to Yes by default. If you select No, scans are not synced to the cloud.
Figure 1. PVT settings
Click
The following table shows a series of conditions that would prevent a scan from
syncing or not:
| Settings in Sync Status | Work Hours | Project Sync Status | Will the project Sync? |
|---|---|---|---|
| Disable | * | * | No |
| Enable | Yes | * | No |
| Enable | * | External file | No |
| Enable | No | Not external file | Yes |
Note: An external file refers to any scan that is not
perfomed on the PVT application but imported into the PVT from a .pvt file or downloaded
from the PVT Dashboard.
Note: This option is hidden by default. In order to display
this option, set the value of
HideSyncSetting=False in
the JCI.Applications.PVT.exe.config file located in
C:\Program Files (x86)\Johnson Controls\Metasys
Performance Verification Tool.