Using PVT in automatic scan mode - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.3

Metasys Performance Verification Tool (PVT) User Guide

Brand
Metasys
Product name
Performance Verification Tool
Document type
User Guide
Document number
LIT-12012406
Version
4.3
Revision date
2023-07-27
Language
English

Use the automatic scan mode to schedule scans to automatically occur at a defined interval. The data is uploaded to the PVT cloud and is available for display through PVT Dashboard reports.

You also have the option to do on-demand scans, view and export scan data, generate scan reports, delete a scan, and compare scans.

Note: In autoscan mode, the following functions are not available: updating and editing scans, saving scans as a PVT file, exporting a riser, and refreshing results.
Note: Automatic scan mode is only accessible to users with Johnson Controls credentials.
Note: After automatic scans are scheduled, opening PVT in Interactive Mode cancels an in-progress auto scan.
Note: There is no scan type in Autoscan mode. It scans Inventory, Performance and Assessment data by default.
Note: You can only use Autoscan mode with an internet connection, so it is not possible to store files locally and manually upload those to the dashboard.