To install PVT successfully, we recommend the following hardware and
software configurations:
- Desktop operating systems:
- Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit).
- Server operating systems:
- Windows® Server® 2016 with Update (KB4512495) (64-bit)
- Windows® Server® 2019 (version 1809 or later) (64-bit)
- Windows® Server® 2016 (version 1607 or later) (64-bit)
- Connectivity
- Internet connectivity of 5 Mbps or greater to sync PVT scans to cloud without interruption (Autoscan mode)
- Configuration:
- <15 Engines: 8 GB RAM
- 15-25 Engines: 16GB
- 25 or more engines: 32GB Note: Ensure an additional 8GB of RAM is available to run PVT on a Metasys server machine.
- 100 GB HDD
- Microsoft .Net 4.7.2 or above
- Microsoft Office® 2010 or above
- Microsoft Visio® 2013 or above for exporting Riser view
- SQLite® v3.27.2
Data Points in Autoscan mode
When PVT is installed on a Metasys server, the following server machine
data points are captured by PVT:
- Server Machine RAM usage
- Server Machine CPU usage
- USB port status
- OS version
- Hard drive free space
- Firewall status
- SQL version
Note:
- If the Software Manager and SQLite v3.27.2 do not exist on the computer, the PVT installer automatically installs them during PVT installation. You do not need to remove any other SQL Server version that is installed on the computer.
- If you install PVT on a server that runs ADS or ADX, the system requirements must match those outlined in Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525).
- PVT UI works best with resolution settings 1920 x 1080. For the best viewing experience, set size of text, apps and other items to 100%.