Exporting the riser diagram - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24

About this task

When you open a scan, you can export a riser diagram of the scanned devices into a Microsoft Visio file.

Note: This function is available only for inventory and performance scans. You must have Microsoft Visio 2013 or above installed for this process to work.

Procedure

  1. Open a scan. Click Open Scan in the toolbar or main menu, or click on the card of a recent scan in the main PVT window.
  2. Click Export Riser in the upper right.
  3. Microsoft Visio opens and the riser diagram is automatically created.